Pascal Lepretre

Pascal Lepretre

  • Connect with me
  • RSS
I graduated in Electrical Engineering in 1986 and obtained a degree in Technical Innovation and Management in1999. I joined Merlin-Gerin in 1986, working on the design of high power, low voltage circuit breakers. Since 1994, I belong to the Advance Development team of the Switchboard and Busbar Systems division of Schneider-Electric.

How Electrical Conductivity and Temperature-rise Limitations Impact LV Switchboards

4.6K views 0 0 143

With IEC 61439, Assure Thermal Stability and Reliability in Low Voltage Electric Switchboards

8.1K views 0 0 186

Ensure Short Circuit Withstand Strength in Low Voltage Electric Switchboards

8.3K views 0 0 237

IEC 61439: Ensure Insulating Material Properties To Protect Electrical Panels

6.8K views 9 0 261

Clearances and Creepage Distances in LV Electrical Switchboards

13.1K views 1 1 490

IEC 61439: Rated current of Electrical Panel and Switchboard Protection Devices

10.6K views 5 3 453

Avoid the Wrong Type of Electrical Fireworks with IEC 61439

7.7K views 4 2 223

Circuit breaker: derating is not downgrading

19.5K views 450 15 4.6K

Aluminium: Inherently good for bus bars

39.4K views 598 4 5.3K
IEC standard 61439

IEC 61439, More than just an upgrade, a whole new approach

7.9K views 39 0 1.2K