Paul Desmond

Paul Desmond

  • Connect with me
  • RSS
Paul Desmond is an award-winning writer who has been involved in the IT trade press since 1988. Paul spent 11 years at Network World, serving as a reporter as well as news editor and features editor. Under his leadership, Network World’s features department took home a number of editorial excellence awards, including a 1996 Neal Certificate of Merit Award from the Business Press Association and two 1998 awards from the American Society of Business Press Editors. Paul has also served as editor of Redmond magazine and was the founding editor-in-chief of Redmond Channel Partner magazine, which earned a Neal Award for Best Startup publication of 2005. He has been writing and developing content for MediaSolve Group since 2011.

Key Elements of a Data Center Growth Model

5.8K views 0 0 1.0K

4 Keys to Creating an Energy-Efficient Data Center

5.9K views 0 0 889

5 Contributors to Data Center Energy Inefficiency

10.4K views 0 0 726

5 Essential Components of Data Center System Planning

14.0K views 0 0 2.2K

4 Potential Drawbacks of Data Center Facility Modules

10.0K views 0 0 1.8K

Success in Data Center Projects Requires Defining These 3 IT Parameters

5.6K views 0 0 761

Save Time and Money with Data Center Facility Modules

4.7K views 0 0 865

3 Common Errors To Avoid When Commissioning a Data Center

4.7K views 0 0 1.0K

Proper Planning Includes Preparing for the Unpredictable

4.1K views 0 0 603

Standardizing the Process of Creating a Data Center

4.2K views 0 0 747

Allocating Energy to IT Users

4.1K views 0 0 717

Allocating Data Center Energy Costs and Carbon to IT Users

4.3K views 0 0 760