Maurizio Rovaglio

Maurizio Rovaglio

  • Connect with me
  • RSS
Maurizio Rovaglio studied Chemical Engineering and holds a Master and a PhD in the same area. He holds multiple patents and has authored over 100 technical articles published on International Scientific Journals, and has presented in multiple International Conferences. Maurizio brings over 25 years of experience in Software Sales, Marketing, Resource Planning and Project Execution in the O&G domain across the world. An enthusiastic leader, he is a true advocate of continuous improvement. Maurizio has also provided major industry players with consulting services including technical advice, advanced control and performance monitoring solutions. A passion for knowledge-sharing has led to almost 20 years of experience as a University Professor in the prestigious Politecnico di Milano, where he lectures various control, instrumentation and process design courses. Maurizio is a specialist in the fields of IIoT, Virtual Reality Applications, Simulation, Process Control, Manufacturing Execution Systems, Performance Monitoring, Optimization and Managing Information Systems in Refining, Petrochemical and Chemical Industries.
digitization

How Convergence of Power & Process Management Systems Benefits the Oil & Gas Industry

4.3K views 7 0 587

Methods that Facilitate Oil & Gas Power & Process Management Systems Convergence

4.8K views 25 0 788

Why Oil and Gas Companies are Driving Towards Convergence of Power and Process Management Systems

5.1K views 10 0 592
cybersecurity

Uncovering Cybersecurity and the IIoT in Oil & Gas Business

5.4K views 0 2 738
IIoT control maintenance

Bringing Innovation to Every Level of the Oil & Gas Sector

5.2K views 10 0 784