Michel Prunier

Michel Prunier

  • Connect with me
  • RSS
From a technical point of view, Michel participated in the establishment of the first technology programmed into the reactor safety system (nuclear island) to replace analog technology. As a result he worked to drive the replacement of analog to digital technologies in existing plants (neutron flux system and conventional I&C). These experiments were put to use in the field of national defense and especially the Navy and in civilian critical systems (railway as an example).

Safety Certification is Key to Nuclear Power Expansion

5.6K views 6 0 580