Mark Chidichimo

Mark Chidichimo

  • Connect with me
  • RSS
I'm Offer Director, Power Solutions for Data Centers. Diverse and extensive background within critical power industries with keen understanding on why availability and reliability are important! MBA - The University of Calgary B.Sc., Mechanical Engineering - University of Illinois at Urbana-Champaign

The Domino Effect: How energy efficiency in Data Centers may lead to power factor issues

13.0K views 7 29 2.2K

Machines that go PING: Getting the most from your power monitoring system

5.9K views 4 0 930

INFOGRAPHIC: Here is the Data on Data Center Energy

9.2K views 17 5 1.1K

Automated testing takes your backup generators ‘to the wall’

8.7K views 4 0 873

How fast is fast? Power monitoring and real-time response rates

7.5K views 5 1 852