Lorène Grandidier

Lorène Grandidier

I'm a graduated in Marketing Management of Grenoble Business School (ESC Grenoble), France. I have experience in industrial marketing and I was involved in the Shore Connection activity for Schneider Electric, managing strategic marketing and institutional relationships. I'm part of T&D Europe Association, under Orgalime, involved in the Task Force Harbor.

Why is a regulation required for developing Shore Side Electricity and greener ports?

44.9K views 62 1 4.1K

Are Scrubbers a relevant solution for shipping industry?

23.3K views 22 4 4.4K

California US: the platform of shore power development

9.1K views 12 0 1.5K
Shore Connection, GreenPort Asia Mumbai, March 2013

Green port is coming to Asia

7.0K views 1 0 1.0K