Constantine Lau

Constantine Lau

  • Connect with me
  • RSS
Constantine Lau is a Global Director of Oil & Gas Segment with Schneider Electric, and holds 20+ years of experience in Industrial Automation and Software. He is responsible for oil & gas segment business strategies and sales and marketing programs. Constantine had published numerous articles on advanced software topics such as, advanced process control & optimization, AI systems, and Fieldbus. He graduated with dual engineering degrees from the University of Texas, and MBA from the University of Houston.

Process Energy Optimization – Improving Bottom Line and Sustainability

2.3K views 0 0 76

Demystifying Industry 4.0

2.8K views 2 0 68

Power System Optimization Reduces CAPEX and Improves Plant Availability

1.5K views 0 0 42
oil and gas

Higher Return on Capital Employed (ROCE) in Oil & Gas Downstream Operations Part One: Decreasing CapEx

4.3K views 3 0 220

Safety Is Sustainable and Profitable

4.8K views 0 0 252

The next industrial revolution in IIOT and digitization will be vital in helping oil and gas companies to improve their sustainability strategy

5.5K views 7 7 314