Kristian Langborg-Hansen

Kristian Langborg-Hansen

  • Connect with me
  • RSS
I work with development of Schneider Electric's software offer for data centers. My primary focus is supporting customers in improving the energy efficiency of their data centers. In Schneider Electric, I've been developing the Energy Efficiency module for Struxureware Data Center Operation and tools for performing the assessments of the Energy Management Service. Prior to joining Schneider Electric, I was a self-employed consultant working for major private and public organizations. Feel free to follow me on Twitter: @klangborg

The environmental impact of running software

9.5K views 17 1 1.1K

Don’t miss the Gorilla in your Data Center

5.4K views 4 0 761

Winning the Data Center Marathon

5.5K views 0 17 553

The hidden cost of cooling redundancy

5.1K views 0 0 917

Following the moon

4.5K views 0 0 742

This is written using recycled bits

4.9K views 0 0 901

Who cares about carbon emissions?

6.1K views 9 0 852