Jacques Schonek

Jacques Schonek

  • Connect with me
  • RSS
Jacques Schonek graduated from the University of Toulouse, France, with a doctorate in Electrical Engineering. He took part in the development of Telemecanique variable-speed drives from 1980 to 1995. He was subsequently in charge of studies in the field of Harmonic Filtering and Electrical Distribution architectures and later in charge of developing solutions for the Water segment of Schneider Electric. He was also responsible for Knowledge Management for the Power Factor Correction line of business of Schneider Electric.
renewabe-energy-wind-mills-solar-panels-small

Some figures about renewable energy

6.6K views 28 23 1.1K
Monitor for a better Energy Efficiency

What are the most important electrical parameters to monitor for a better Energy Efficiency?

19.6K views 8 3 2.1K
kvar, Kw, PF

KVAR, kVAr, … or kvar?

78.0K views 41 18 5.7K

How big are Power line losses?

107K views 52 55 5.8K

How to illustrate "Reactive Power"?

13.6K views 3 0 1.1K

Did you know that it is possible to save CO2 by connecting capacitors to the electrical networks?

17.1K views 11 17 2.0K