Juha Rintala

Juha Rintala

  • Connect with me
  • RSS
Juha Rintala received his B.Sc. degree in information technology from University of Applied Sciences in Vaasa, Finland, in 2006. He currently works at Vamp Oy/Schneider-Electric as offer manager/AED expert in arc-flash protection and has held the roles of HW design engineer and after-sales engineer/arc-flash expert.

4 Steps for Testing and Commissioning Arc Flash Protection in Medium Voltage

9.1K views 3 0 562

3 Best Practices for Arc Flash Protection in Medium Voltage Equipment

11.1K views 535 7 943

Arc Flash Protection Benefits in Medium Voltage

16.0K views 0 0 1.1K

The Goal of Medium Voltage Arc Flash Protection: Safety Standards

16.1K views 1 0 1.1K

Arc-flash protection options and GOOSE communication

13.7K views 671 91 2.0K