Josep Lopez

Josep Lopez

  • Connect with me
  • RSS
Josep López is leading the strategic view on Thermal Management roadmap in Universal Enclosures business within Schneider Electric. On areas like strategic marketing, business development, innovation & project management is providing an strong vector in this company.

Mastering the art of control panel thermal optimization

981 views 1 0 153

How Smart Fan Filters Help Save Money and Energy

2.4K views 4 0 65

Replace the Control Panel Fan Filter to Save Money and Equipment

2.7K views 1 0 96

Prepare for the Winter Corrosion Speedup

3.9K views 96 0 624

Air-water Exchangers Keep Things Cool

4.9K views 56 0 656

Can Design Offices Challenge the Limits on the Thermal Specifications of a Project?

4.9K views 50 4 838

With ClimaSys DT, System Integrators Keep Their Cool

4.7K views 63 0 837

Getting Maximum Reliability out of Onboard Control Panels

5.4K views 71 0 688

A Cold Answer to High and Stringent Cooling Demands

4.7K views 26 0 671

Heaters: A Hot Topic

15.2K views 27 6 1.1K

Thermostats: Maximizing their Usefulness

14.5K views 27 0 878

Secrets of Reliable Ventilation

6.3K views 23 0 967