Jordan Lerner

Jordan Lerner

I am a high-energy, committed, responsible, outside-the-box innovator and professional energy efficiency activist, coach and collaborator. I have more than 20 years of experience in the energy efficiency and construction industries. My home is the beautiful city of Seattle with my beautiful wife and two amazing daughters. I enjoy a great hike with my faithful canine buddy, Ben.

Schneider Electric Project Selected as APWA Texas Chapter Project of the Year

7.0K views 585 54 1.2K

With Deferred Water and Wastewater Maintenance – Pay the Piper or Pay it Forward

7.1K views 36 0 987

Municipal water and wastewater utilities find silver lining of drought

8.4K views 4 5 1.1K