Jerome Guillet

Jerome Guillet

I currently assist projects at early stage, regarding large motor applications. As the optimum of the whole is not equal to the sum of local optima, the aim is to optimize Customer solution in a global approach. It widely includes electrical distribution considerations, motor specifications and application requirements, and concerns normal conditions as well as fault situations. Since 2015, I had grown my expertise as part of Motor Management Competency Center team (M2CC), and made analysis with EMTP-ATP transient software. I also developed calculus tools and trainings around the subject.

How to estimate electrical network stress during large motor starting in pre-design phase

952 views 0 0 34

Avoid electrical network stress during large motor starting using simplified calculations at design stage

904 views 1 0 26
power factor correction motors

3 safety measures for motors with individual power factor correction

14.9K views 10 0 814