Jaimie Giarrusso

Jaimie Giarrusso

Jaimie Giarrusso manages the global strategic marketing communications for the EcoXpert Partner Program of Schneider Electric. Mrs. Giarrusso has executed several successful marketing communication and brand campaigns, pioneers digital marketing initiatives, and has managed numerous global events. Additionally, she has established an effective collaboration with regional field marketing teams to align local efforts with corporate objectives. Married with two children, Mrs. Giarrusso has a degree in Business Management and is intrigued by other cultures, traditions, and societies.

Wireless technology is changing the playing field for building owners. That’s cool.

20.9K views 1.2K 772 2.0K

Energy efficiency – the new mark for hotel excellence and a real ROI

19.3K views 135 23 2.7K

Why application-specific controllers are changing the playing field for zone-level control

8.7K views 273 28 1.5K

How to optimize your lab’s energy efficiency without compromising its compliance or safety

14.4K views 728 13 2.3K

Medical research improved through efficient laboratory workplace settings

11.3K views 133 16 2.1K

Do You Like a Challenge? Take this Ecological Footprint Quiz!

16.9K views 12 133 1.3K
Schneider Electric Bio Safety Levels

Bio-safety: Securing More than Deadly Viruses – Securing the Bottom Line

10.5K views 6 1 1.4K

Six Ways Running a Marathon is like Reducing Energy OpEx

9.4K views 7 30 1.4K

30%? 8%? What do these numbers mean for energy efficient buildings?

7.5K views 8 3 884

Active Energy Management: The Right Prescription for Pharmaceutical Manufacturing Plants

57.2K views 24 8 2.2K

Money talks. Are you listening?

16.6K views 14 17 1.5K

Facts & Stats – Global Warming 101

11.5K views 0 0 1.3K