Jane Braun

Jane Braun

  • Connect with me
  • RSS
Jane Braun is a 25 year Schneider Electric employee with experience in both the Industry and Buildings businesses. After receiving two Masters degrees from Boston University Jane was a Boston cable news anchor and subsequently a newspaper reporter. The colorful part of her career was in the 80s as the PR Manager for the rock band Boston during their Third Stage album comeback.

Go with the Flow to Select the Right Valve

5.0K views 2 0 1.0K

Don’t Sweat Temperature Taking

4.2K views 20 0 743

Actuators: Remove Failure as an Option

6.4K views 10 3 879

Want Holistic HVAC and a More Effective BMS? Think Field Devices

7.4K views 535 45 1.2K

CO2 Sensors, Goldilocks, and Creating a Building Management System that Works Just Right

19.2K views 4 1 1.0K

Field Devices: Case Studies in Controlling Costs and Increasing Comfort

5.4K views 16 0 930

Build a Firm BMS Foundation with Field Devices

6.4K views 38 1 985