Jane Braun

Jane Braun

  • Connect with me
  • RSS
Jane Braun is a 25 year Schneider Electric employee with experience in both the Industry and Buildings businesses. After receiving two Masters degrees from Boston University Jane was a Boston cable news anchor and subsequently a newspaper reporter. The colorful part of her career was in the 80s as the PR Manager for the rock band Boston during their Third Stage album comeback.

Prepare Your Home to be Smart

5.2K views 154 0 700
KNX Multitouch Interface for Smart Homes

The Interface is the Solution for Smart Homes

5.6K views 15 47 884

The Role of Device Level Control in Hospitals

6.0K views 34 0 786

Is the School Building BMS Ready for School To Begin?

4.8K views 12 0 776

The Internet of Things and Device Level Control

6.3K views 29 1 696

Schools: Avoid Over- and Under-Conditioned Air

6.4K views 7 0 780

Trends in Device Level Control: Valves and Actuators in School

5.5K views 0 0 796

Trends in Device Level Control: Sensors in School

4.4K views 0 0 676

Valves Deserve Some TLC

3.9K views 6 0 643
Schneider-Electric-Valves-and-Actuators

If Valves and Actuators Aren’t Healthy – Neither is the BMS

6.4K views 35 0 775

Save Energy and Boost Educational Spending

7.7K views 29 100 964

Valves: Unseen and Unsung Heroes

5.1K views 48 0 709