Jaimie Giarrusso

Jaimie Giarrusso manages the global strategic marketing communications for the EcoXpert Partner Program of Schneider Electric. Mrs. Giarrusso has executed several successful marketing communication and brand campaigns, pioneers digital marketing initiatives, and has managed numerous global events. Additionally, she has established an effective collaboration with regional field marketing teams to align local efforts with corporate objectives. Married with two children, Mrs. Giarrusso has a degree in Business Management and is intrigued by other cultures, traditions, and societies.
5 min read

Today’s Lesson Plan: The Evolution from Pinocchio to Wireless Technology in K-12 Schools

9.1K views 45 0 1.7K
3 min read

Easy & Affordable: Optimizing Efficiency in Retail Healthcare Clinics

7.9K views 521 0 1.3K
4 min read

An Alternative to Building Management Systems for Smarter, Safer, and More Efficient Schools

7.1K views 32 0 1.2K
5 min read

A “connected” hotel not only enhances your guests’ stay…it delivers a virtually immediate ROI. Best part is…it’s easier than you might think.

15.5K views 730 0 1.7K
4 min read

Floating Mylar balloons – the latest technology in hotel comfort. Really?!?! Some believe so…

12.7K views 19 0 1.9K
4 min read

Who doesn’t want a better learning experience for their children? I know I do!

8.0K views 18 0 1.4K
1 min read

Wireless technology is changing the playing field for building owners. That’s cool.

23.8K views 1.2K 0 2.4K
2 min read

Energy efficiency – the new mark for hotel excellence and a real ROI

21.3K views 135 0 3.0K
2 min read

Why application-specific controllers are changing the playing field for zone-level control

10.6K views 273 0 1.9K
2 min read

How to optimize your lab’s energy efficiency without compromising its compliance or safety

16.3K views 728 0 2.7K
1 min read

Medical research improved through efficient laboratory workplace settings

13.2K views 133 0 2.4K
2 min read

Do You Like a Challenge? Take this Ecological Footprint Quiz!

18.7K views 12 0 1.6K