Gregory Bouchery

Gregory Bouchery

  • Connect with me
  • RSS
Grégory Bouchery joined Schneider Electric in 2007, as automation trainer & country marketing manager in Japan. After being involved in the business incubation of the Pelco video security solutions & energy management solutions in Japan, he joined the worldwide Control & Signaling marketing team. Since then he is located in the Angoulême, France, and is in charge of future offer creation.

Even more practical tips for enhanced ergonomics and design for operator interfaces

1.4K views 0 0 93

More practical tips for enhanced ergonomics and design for operator interfaces

1.6K views 2 0 88

Practical tips for enhanced ergonomics and design for operator interfaces

1.6K views 2 0 81

Save installation time: round holes are not only for pushbuttons

2.5K views 3 0 138

Plastic or Metal: What’s Driving the Choice of Pushbutton Materials?

4.0K views 4 0 158

How to get on the road to Smart Machines: The ABC’s of control interface ergonomics

3.7K views 2 0 310

Do you Speak Robustness-ish? Pushbuttons for Food and Beverage Applications!

5.0K views 2 0 325

Machine Aesthetics : A Simple Guide to Pushbutton Fashion!

5.2K views 0 0 290

The Truth Behind the Colors of Pushbuttons

9.4K views 9 0 429

The ABC’s of Emergency Stop Buttons…A Simple Concept that can get Really Complicated

7.8K views 2 3 369

Do you Speak Robustness-ish? IP Protection Levels

4.8K views 44 0 367

How to get on the road to Smart Machines: The ABC’s of Alarm Management

15.5K views 29 0 625