Fabio Mielli

Fabio Mielli

  • Connect with me
  • RSS
Fabio Mielli, 41, is the U.S. Mining, Minerals, and Metals Segment Manager for Schneider Electric. He has 20 years of experience in power, speed drives, automation, and industrial control, and has worked closely with the major mining and metals producers. Fabio has published as author or co-author more than 20 articles and papers related to automation, energy and industry trends related to the mining, metals and minerals segments and their challenges and applications.

Roadblocks to watch out for on the path to Digital Transformation (Part 1?)

4.7K views 20 0 178

Is Digitization and IoT a New Thing? Not if you come from Industrial Automation

8.5K views 919 17 506

The Sky is the Limit? When Mainstream Digital Technology Meets the Mining Industry

4.7K views 72 9 611

5 Reasons Why the World Needs Mining …And Always Will

26.5K views 386 64 2.0K

The use of mobile technology for maintenance, safety and environmental inspections

6.6K views 40 19 1.2K

Virtual reality training for mineral processing plants

12.2K views 594 13 3.2K

Advanced Process Control and Mineral Processing Applications

9.6K views 519 3 2.1K

The internet of things (IoT) and….. Mining operations?

18.1K views 53 53 4.2K

Water Management for Mining Operations: The big challenges and potential (technical) solutions

9.6K views 44 0 1.7K

The Mill of the Future and Technology Enablers

10.6K views 18 0 1.1K

Process control requirements for a Steel Mill (and some myths)

13.9K views 17 0 1.6K

Top challenges faced by the mining industry and its implications (Part 2)

18.8K views 11 2 2.1K