Didier Mignardot

Didier Mignardot

I have been interested in lightning and ways of protecting people and buildings from its destructive powers for over 20 years. A founder member of the French Association of Protection against Lightning (SPD), I am currently marketing manager in Schneider Electric’s Surge Protection Department. I helped draft the surge arrester installation guide UTE C15443 and was a member of the working group that draw up IEC standard 60364-4-443 and the 5-534 update. I have also authored a number of publications on lightning.

Lightning surge protection: Two is better than one!

51.9K views 42 20 4.1K

6 facts and fictions about lightning

26.1K views 13 82 2.2K

Length, the critical parameter in installing surge arresters

28.0K views 4 3 3.4K

How to choose the right surge protector?

96.5K views 9 10 5.4K
Arresting the surges in lightning strikes

Arresting the surges in lightning strikes

33.2K views 11 21 3.6K