Daniel McGinn

Daniel McGinn

  • Connect with me
  • RSS
Daniel McGinn is the Director of Secure Power Systems at Schneider Electric. In his role, Dan is responsible for business development strategies and execution in the area of UPS and related technologies for the Industry and Infrastructure spaces. Dan works across multiple business units within Schneider Electric to address the Secure Power needs of varied market segments. Dan has over twenty years experience as a business and technology professional in the arena of Process Automation, Energy Management and Manufacturing IT systems with extensive experience in the application of UPS technology including 3-phase systems and redundant power generation. Daniel has a Bachelor of Science degree in Electrical Engineering from the University of Michigan at Ann Arbor.

How to Provide IIoT Power Protection in an Industrial Internet of Things Environment

16.7K views 27 0 1.7K

Why are there more power outages than ever and how can the impact be averted?

7.8K views 15 0 979

Integrating IT, OT and Security: The Power Imperative

7.1K views 19 2 888

Integrating IT, OT and Security: Convergence to Collaboration

9.6K views 36 61 998
IoT

It’s Time to Give IOT and Edge Infrastructure the Same Protection IT Resources Get

8.0K views 9 0 827
business continuity

As IT meets OT, a Cultural Shift is Required to Ensure Business Continuity

7.2K views 14 0 941

Critical Systems Protection in Healthcare: Your Guide to Risk Assessment

8.1K views 89 1 1.1K
Critical Power

UPS Deployment Strategies for Critical Power Distribution

97.1K views 27 0 1.3K

The Internet of Things Demands New Thinking about Power Protection for Mains and Brains

8.3K views 507 0 1.1K

Determining the ROI of UPSs Requires a Comprehensive Risk Analysis

8.1K views 23 0 1.3K

5 Places Where Critical Power Plays a Crucial Role

9.3K views 112 19 2.0K