Duke Dunsford

Duke Dunsford

  • Connect with me
  • RSS
Duke Dunsford is currently Marketing Offer Launch Leader in the Partner Projects division, handling offer launches for the USA market. His concentration is on communicating devices for Low Voltage power distribution equipment. Duke joined Schneider Electric in 2008, and was formerly Product Manager for MVP lighting & final distribution panels utilizing high density branch circuit power metering. He also coordinated the development of Schneider Electric’s Energy Insight software solution for aggregation and visualization of MVP high density metering. Duke is passionate about providing the information users need to utilize their electrical power resources as efficiently as possible.

What Keeps Facilities Managers up at Night: And How You Can Avoid Counting Sheep Yourself

29.4K views 395 0 1.5K

Hello, Facility Manager? This is Circuit Breaker No. 4

11.6K views 746 11 1.4K

Kicking the Break/Fix Habit with Asset Management

6.5K views 339 1 891