Daniel Desruisseaux

Daniel Desruisseaux

  • Connect with me
  • RSS
Dan DesRuisseaux is a Cybersecurity Offer Manager within Schneider Electric’s Industry business unit. Dan has over 25 years of experience in defining, marketing, and selling technical products and solutions. Core responsibilities include creating cybersecurity strategy, driving cybersecurity features in product line roadmaps, and working with best in class partners to improve solution security.

TIPs to Effectively Maintain Industrial Control System Security

13.5K views 2 1 232

TIPs to Securely Deploy Industrial Control Systems

6.2K views 1 0 231

Modbus Security – New Protocol to Improve Control System Security

9.6K views 3 1 429

I Want to Secure My Industrial Control System – What’s the First Step

6.1K views 2 1 259

Cyber-Nationalism in Cybersecurity Standards

6.0K views 2 0 341

IEC 62443 Security Assurance Levels Explained

23.5K views 6 0 928

Value of a CyberSecurity Certificate

15.8K views 88 11 884

Reducing Vulnerability to Cyberattacks

14.7K views 69 0 845
Partnering Security

Partnering with Specialists to help Protect the World’s Critical Infrastructure from Cyber Attacks

8.3K views 235 13 1.1K
cybersecurity training

Building Cybersecurity Knowledge Is Critical First Step to Secure Industrial Networks

16.9K views 75 0 859

The Cybersecurity Business Case: An Arduous Challenge – Part 2

16.3K views 9 0 709

The Cybersecurity Business Case: An Arduous Challenge – Part 1

18.2K views 7 41 1.0K