Daniel Barstz

Daniel Barstz

  • Connect with me
  • RSS
Systems Architect at Partner/Strategy/Technology, I am a recognized Edison expert. I hold an MBA, I developed and managed the worldwide IEC intelligent MCC offer during several years, and I am the author of several patents linked to the design and performance of intelligent switchboards. I have been working with critical continuous process industries like Oil & Gas, Mining, Aluminium, Steel, Water treatment, etc. for more than 30 years.
ETHERNET NETWORK IN ELECTRICAL DISTRIBUTION

Ethernet network in Electrical Distribution

10.0K views 776 16 1.3K
daisy chain

Daisy Chain: the redundancy star of topology

14.2K views 6 0 1.8K

Redundancy puts backbone into the ring topology

15.1K views 52 5 2.0K
Auxiliary power systems iPMCCs

Coherent place for auxiliary power system in iPMCC

10.4K views 13 0 865