Brian Milne

Brian Milne

Milne manages the refined fuel’s editorial content, spot price discovery activity and cash market analysis for Schneider Electric’s energy segment. Milne has 20 years’ experience in the energy industry as an analyst, journalist and editor, serving as Managing Editor for Btu publications and journalist with Bridge Information Systems America. His industry and market focus include natural gas, NGLs, electricity during its move to deregulated markets in the late 1990s, biofuels, and the downstream petroleum industry. He has been quoted in national media outlets that include The Wall Street Journal, USA Today, Barron’s and Newsweek and regularly provides industry commentary for media including Convenience Store Decisions and Biofuels International. Milne graduated Magna Cum Laude from Monmouth University in New Jersey with a B.A. in History and an Interdisciplinary in Political Science.

Strong Run Rate Coincides with Higher Gasoline Demand

6.0K views 0 0 1.6K

Gasoline futures hit seasonal spike

4.2K views 0 0 625

RBOB Futures Steps on the Gas in Ushering in March

5.1K views 0 0 1.2K

Have Gasoline Futures Reached a Bottom?

6.7K views 0 0 916

Lowering the Bar in Oil’s Limbo Dance

7.0K views 0 0 1.3K

Sub $2 Gasoline and Robust US Vehicle Sales

5.4K views 2 0 1.5K

US Gasoline Demand Trends Higher in October

4.8K views 5 0 942

US Gasoline Futures Driving towards 2015 Low

4.3K views 8 0 921

Gasoline’s Seasonal Change and Market Volatility

5.0K views 6 14 901

Pedal to the Metal, as Low Gasoline Prices Spur Driving Demand

4.6K views 2 3 894

Just a Tryst, or have Americans again Fallen in Love with the Automobile?

4.9K views 5 4 802

Is Late May Surge in US Gasoline Demand Sustainable?

5.4K views 3 3 853