Brian Milne

Brian Milne

Milne manages the refined fuel’s editorial content, spot price discovery activity and cash market analysis for Schneider Electric’s energy segment. Milne has 20 years’ experience in the energy industry as an analyst, journalist and editor, serving as Managing Editor for Btu publications and journalist with Bridge Information Systems America. His industry and market focus include natural gas, NGLs, electricity during its move to deregulated markets in the late 1990s, biofuels, and the downstream petroleum industry. He has been quoted in national media outlets that include The Wall Street Journal, USA Today, Barron’s and Newsweek and regularly provides industry commentary for media including Convenience Store Decisions and Biofuels International. Milne graduated Magna Cum Laude from Monmouth University in New Jersey with a B.A. in History and an Interdisciplinary in Political Science.

Preseason Rally for US Gasoline Futures so far Muted

4.8K views 0 0 677

US Gasoline Futures Drop Back in Spring Transition

5.2K views 0 0 705

Gasoline’s Bull Charge into 2017

4.9K views 0 0 574

The market was gloomy in 2016, but OPEC cut provides some hope in 2017

5.0K views 2 0 579

Trump and the US Biodiesel Market in 2017

6.1K views 1 4 1.3K

Gasoline Futures Surge 12% in December to New High

5.0K views 0 0 956

Is the US Gasoline Market Defying the Seasonal Downturn?

5.5K views 0 0 722

US Gasoline Prices Spike in Response to OPEC Deal

5.9K views 0 0 768

U.S. Biodiesel Industry Again Waiting on Government Largesse

5.3K views 0 0 658

Colonial Pipeline Explosion Spikes Gasoline Futures

6.2K views 0 0 1.1K

Recent Surprises Turn Oil and Gas Market Bullish

5.1K views 0 0 871

US Gasoline Market’s September Surprise(s)

8.6K views 0 0 873