Bernard Jover

Bernard Jover

I am a senior expert in electromagnetic compatibility (EMC) with Schneider Electric where I’ve worked since 1988 and built up my expertise in lightning protection. I’m a power electronics graduate with a speciality in training that I obtained at the Ecole Polytechnique – a well-known technical university in France. On graduating I worked as a design engineer before joining Schneider Electric in the late 1980s. Over the years I’ve built up a body of knowledge and expertise in electromagnetics and protecting installations from lightning – particularly hardening methods and processes. I have led lightning protection studies, performed diagnostics, and designed solutions in fields of industry ranging from military applications to the food and beverage business. I am particularly interested in standards and as a specifications engineer and I actually have two patents to my name. I have been an active member of the European Committee for Electrotechnical Standardization for 15 years and I’m also a member of the French national body. I do a lot of teaching and training, too. I think it is as important to share expertise as it is to acquire it.
The world of electronics can be a cruel one for cables – particularly the sensitive ones that carry sensor readings. They can be badly disturbed by the big power cables or relay switch arcs.

Happy families are segregated families in cabling

9.1K views 310 39 1.4K

Cable management systems for Electromagnetic emission control

8.5K views 691 8 1.4K
Cable management systems

Foil tour coils with TVS to protect the integrity of your communications

6.5K views 290 1 1.0K
ElectroMagnetic Compatibility (EMC)

Electromagnetic Compatibility (EMC) standards: review of the requirements

13.6K views 144 2 2.5K
ElectroMagnetic Compatibility (EMC)

Electromagnetic disturbances: communications networks particularly sensitive

8.6K views 95 1 1.3K

Choosing the right earthing system

20.6K views 175 6 3.9K