Andrea Willman

Andrea Willman

  • Connect with me
  • RSS
Andrea Willman is the marketing manager for Schneider Electric’s Weather division. In her role, she is responsible for all lead generation efforts, targeting both prospective and existing clients. She has served in this role since 2005.

Share the View

4.6K views 0 0 677

2017 Outlook: Doing More With Less in the Downstream Market

5.1K views 0 0 772

eBOLs: Fact, Fiction and Future

5.0K views 0 0 729

Energy Commodities – Are The Bulls Starting To Run?

5.6K views 5 0 735

New-Age Terminals Require New-Age Solutions

5.8K views 6 0 834

The Benefits of Arbitrage

5.8K views 0 0 1.2K

Digital Age Solutions: Impact Your Bottom Line

4.9K views 6 0 788

Re-Sellers: Protect Your Bottom Line

4.7K views 3 0 796

2014/15 Winter Weather Outlook

6.7K views 1 4 1.2K

Weather Risk Forecasting: Don’t Get Caught in a Blackout

5.8K views 14 0 1.1K

Climate Change and Its Effects Part Three: Why Integrating Weather Forecasting is so Important?

5.2K views 1 1 1.0K

Climate Change and Its Effects Part Two: Flooding Trends and Frequencies

6.1K views 2 8 876