Aalok Deshmukh

Aalok Deshmukh

  • Connect with me
  • RSS
Aalok has over 14 years of experience spanning contributions to more than 125 projects in 11 countries, including energy and sustainability implementation, consulting and research experience in the corporate, government and non-profit sectors. He has contributed to several papers and publications and is invited to speak at various events. He has a Masters degree in building science and is a licensed architect in India, a LEED Accredited Professional and a Certified Measurement and Verification Professional.
green building ratings confusion

Making sense of the alphabet soup: Decoding Green Rating systems

4.9K views 19 0 971
energy efficiency

Energy Efficiency as the First Fuel for an Emerging Economy?

8.9K views 0 0 1.7K