Aidin Aliyarzadeh

Aidin Aliyarzadeh

  • Connect with me
  • RSS
Aidin Aliyarzadeh is part of the team for Machine Solutions within Schneider Electric’s Industry business, working as a Technical Trainer for HAVAC& R and Pump applications along with Safety Modules. Aidin joined Schneider Electric in 2006 as part of the Industry Product Marketing team but has been in the field of automation and instrumentation for over 20 years. He is also recognized and awarded as an Edison Solution Architect and holds several patents in the industrial field.

COP Calculation and Monitoring in HVAC Application

28.0K views 10 0 3.7K

Mobile Storage in Industrial Automation Applications

5.6K views 5 0 1.0K

What does “Energy Savings” mean in the industrial automation field?

12.1K views 5 5 2.0K

Less Effort, More Gain…by Dynamic and Colorful Power Monitoring

6.9K views 18 1 1.2K

Your application is always awake

6.7K views 14 1 1.1K