Abderrahmane Agnaou

Abderrahmane Agnaou

  • Connect with me
  • RSS
I'm Thermal Architect for Electrical Enclosures offer at Schneider Electric since 2007. I graduated from ENSEM (Ecole Nationale Supérieure d'Electricité Et de Mécanique), Nancy in France.

[INFOGRAPHIC] 6 steps to optimize outdoor electrical installations

10.0K views 653 23 1.7K

Outdoor electrical installations : determining the right thermal management solution

8.9K views 508 3 1.3K

Electrical enclosures: Warm and dry keeps condensation away

84.1K views 131 18 7.0K
PUE cooling

How to stop control panels losing their cool in summer

15.0K views 52 0 1.9K

What is Thermal Management of electrical enclosures?

19.2K views 36 4 2.0K